As-Interface is a quick and upgradable wiring system, just a single cable required connect all components in an automated system. It contributes significantly to improvement in reliability, availability and machine safety by reducing wiring errors and by offering high-level electromagnetic interference immunity (EMC). The safety function of the machine is totally integrated with AS-Interface Safety at Work.


Simple, economical and reliable
 
The TWIDO and
AS-Interface association offers an easy to use and economical solution, ideal for simple and extended installations and small machines.