Protect Area Design

Protect Area Design software is a configurator that enables selection of the type of safety detection system (mats, light curtains), depending on the application. This software enables the user, via a graphic interface, to create or modify a safe working environment within the vicinity of a potentially dangerous machine.
Having established the predefined fields (selection of control system category, dimensions of the machine), the Protect Area Design software, depending on the reaction time parameters (machine and protection system) and the approach typology, calculates the safety distance and displays the optimal safety detection solution. A list of product references, quantities and accessories to be used is provided.
Protect Area Design software is user-friendly and compatible with Windows 98, NT, 2000 and XP. It is available using product reference SISCD104200, downloadable from our Internet site and included in the Schneider Electric electronic catalogue.