Stop the danger
A complete offer, maximum flexibility
Simple to install
Transmitter-receiver alignment simplified using red LED indicators for each light beam. (An LED indicator on the receiver indicates whether its respective light beam is misaligned and the light curtain is adjusted until all the LEDs are off).


Complete
Integration of fixed blanking, floating blanking, external device monitoring (EDM) and test input (MTS, XUSLT only) functions throughout the light curtain range.
Compact
Compact design light curtains, especially for the Slim range (26 x 30 mm).



Quick connection
Safety and simplicity of cabling using M12 connectors on flying leads that are differently coloured for the transmitter and receiver. (Black for transmitter, brown for receiver).
Software to assist selection
Simple application design using “Protect Area Design” software. This software also incorporates safety mat applications.