|
Safety fully integrated | ||||||
![]() The safety monitor verifies correct operation of the installation and processes the data supplied by the safety devices. In the event of an incident, it renders the machine safe. |
AS-Interface Safety at Work provides the answer to the needs for quick refurbishment. The connection of sensors / actuators is simple due to use of IDCs (Insulation Displacement Connectors). The initiation of the safety functions is performed by the safety monitor, which can be configured using ASISWIN software. |
![]() |
|||||